Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What port to use Communications Port window when using HS0008EAUF1H?

Latest Updated:09/10/2007

Question:

What should I select for a port on a Communications Port window when I use HS0008EAUF1H as an USB adapter board ?

Answer:

Please select FDM for a port.
Suitable Products
HS0008EAUF1H
Flash Development Toolkit