Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

What happen if I use USB to RS-232C to equip my PC?

Latest Updated:10/29/2009


My PC doesn't equip RS-232C. What happen if I use USB to RS-232C converter?


Differ from PC equips RS-232C, USB to RS-232C converter makes it move port via USB, so It might not go well timing synchronizing between FTD and User-System because of timing delay of communication controller. For that reason, we recommend that you should use PC equips RS-232C or use E8a emulator ([R0E00008AKCE00]) can connect to PC via USB. Please check the Flash Development Toolkit target device list, if you would like to refer MCU which has capability of writing with E8a emulator.
Suitable Products
Flash Development Toolkit