Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Flash programming without using Renesas Flash Programmer

Last Updated:05/31/2017

Question:

I want to do flash programming without any existing tools such as Renesas Flash Programmer. Is the communications protocol provided?

Answer:

RX Family

See the section of boot mode in the desired product’s User’s Manual: Hardware.

RL78 Family(except RL78/10)

See the Application Note of RL78 Microcontrollers RL78 Microcontrollers (RL78 Protocol A) Programmer Edition.

RL78/G10

See the Application Note of RL78/G10 Group Programmer Edition.

Suitable Products
RX Family
RL78 Family