Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Meaning of Letters and Numbers in MCU Part Number

Last Updated: 09/10/2015

Question:

Is there a way to decipher what the numbers and letters mean in the part number? How do I decode the MCU part number?

Answer:

Yes, there is meaning behind the letters/numbers which make up the orderable part number. For help with deciphering them, see the available Orderable Part Number Guides below.