Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Bluetooth Smart (Bluetooth Low Energy)

Last Updated: 06/29/2016

Question:

Which MCUs support the Bluetooth® Smart (Bluetooth Low Energy) protocol?

Answer:

The RL78/G1D series of MCUs supports Bluetooth Smart v4.1 connectivity in both embedded and modem modes. The stack is BT SIG qualified with documentation available on the test procedures to facilitate radio certification.


For more information visit our Bluetooth Low Energy solutions page or our RL78/G1D library for sample code and design guides.