Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Serial Communications using the RX63N Microcontroller

Last Updated: 06/30/2016

Question:

What are the various tradeoffs between serial communication standards? Which ones does the RX63N support?

Answer:

In the YouTube video below, Stevan Dobrasevic explains the pros and cons of UART, LIN, SPI, and I2C and providing application examples. He also discusses how the Serial Communication Interface (SCI) peripheral available on the RX microcontrollers can be configured for communication using any of these standards.