Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Amazon Web Services Cloud IoT

Last Updated: 06/27/2016

Question:

Does Renesas have a IoT solution that works with Amazon Web Services (AWS) Cloud Computing?

Answer:

For fast evaluation and prototyping, Renesas, Micrium, and Arrow Electronics have partnered to offer a starter design kit (SDK) YRDKRX63N-AWS based on the RX63N specifically designed to connect with Amazon Web Services' Cloud IoT platform. The YRDKRX63N-AWS is pre-programmed with Micrium's Smart Home Gateway example project which uses Micrium Spectum software to connect to AWS IoT Cloud Platform and is available for purchase through our distribution partners Arrow, Avnet, Digikey & Future.

For information on how to get started and to obtain example projects using the on-board sensors visit www.micrium.com/aws-iot-starter-kit.

 

  • Este artigo foi útil?