Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Renesas Virtual Power Lab Simulation Environment

Last Updated: 6/24/2016

Question:

Does Renesas provide a simulation tool for power applications?

Answer:

Renesas Virtual Power Lab (powered by WebSIM) is a site for performing simulations of the power MOSFET operations of synchronous-rectified buck converters. The tool enables you to calculate waveforms of buck converters or losses of power MOSFETs delivering a regulated voltage to a microcontroller or SOC board. This allows you to select the most suitable power MOSFETs when you start to design, and also helps speed up evaluation.