Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Are there operational amplifiers that can be used with a single power?

Latest Updated:10/01/2006

Question:

Are there any operational amplifiers that can be used with a single power supply?

Answer:

operational amplifiers can be used with a single power supply. Note, however, that the input and output voltage ranges are limited. The input voltage range changes depending on the type of input transistor.
The usable voltage range is listed as "common mode input voltage range" in the Data Sheet. Check the Data Sheet of each product for this voltage range. Note that the specifications with dual power supply are shown in the Data Sheet.
Suitable Products
Operational Amplifiers