Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the thermal resistance of 2SK2415 and 2SK2415-Z?

Latest Updated:09/02/2013

Question:

I'm considering using the 2SK2415 or the 2SK2415-Z. What is the thermal resistance of the package? It's not mentioned.

Answer:

The thermal resistance of the 2SK2415 and the 2SK2415-Z is shown in TRANSIENT THERMAL RESISTANCE vs. PULSE WIDTH on page 4 of the datasheet. Please refer to it.

This article is written based on not recommended products.

Suitable Products
Power MOSFETs for General Switching