Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is 2SK3714-AZ differs from 2SK3714-S12-AZ?

Latest Updated:09/02/2013

Question:

Do characteristics differ between orderable part numbers that contain "S12" and numbers that do not? I don't know whether to order 2SK3714-AZ or 2SK3714-S12-AZ.

Answer:

  • 2SK3714-AZ: Bag packing
  • 2SK3714-S12-AZ: Tube packing

Only the method of packing differs for the above part numbers. The characteristics are identical.

This article is written based on not recommended products.

Suitable Products
Power MOSFETs for General Switching