Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How high can the Zener current go?

Latest Updated:08/01/2005

Question:

How high can the Zener current go?

Answer:

The permissible value of the Zener current varies according to the Zener voltage, the current application conditions (usage conditions), and the mounting conditions.
Concretely, calculate the junction temperature for the actual usage conditions and verify that the absolute maximum rating for the junction temperature (Tj) is not exceeded.
For the concept and junction temperature calculation method, refer to the following document provided on this website.
Precautions Regarding Use of NNCD Series and RD Series
Suitable Products