Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Any alternative/same product with close switching characteristics?

Latest Updated:09/02/2013

Question:

I'm using the UPA1522 in a PWM control (62.5 kHz to 500 kHz) circuit. Compatible current waveforms are important. Is there any substitute/equivalent product with close switching characteristics? It doesn't matter if the package is different. Input capacitance, rise time, and fall time are important.

Answer:

An substitute/equivalent product with close switching characteristics is the 2SK3377.
Suitable Products
Power MOSFETs for General Switching