Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What Zener current value to use to enable the voltage to stable output?

Latest Updated:12/01/2011

Question:

I am considering inserting a Zener diode in my reference voltage circuit.
What Zener current (IZ) value should I use to enable the voltage to be output stably?

Answer:

Use the Zener current value (IZ) described under the Zener voltage (VZ) measurement conditions in the data sheet as a guide.
If the current increases, the amount of heat generated increases, increasing the Zener voltage variation.
If the current decreases, however, the amount of noise generated from the diode itself increases.
Suitable Products