Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the contrast between uPD4066B in CMOS4000 and uPD5200/5201?

Latest Updated:09/01/2007

Question:

What is the difference between the uPD4066B (discontinued) in the CMOS4000 series and the uPD5200/5201?

Answer:

Although both the uPD4066B (discontinued) of the CMOS4000 series and the uPD5200/5201 are CMOS analog switches, they differ widely, as follows.

 

Item uPD4066 uPD5200/5201
Power supply voltage
(recommended supply voltage range)
+3 V to +18 V ±8 V to 16 V
Power system Dual (plus and minus) power supply or
single power supply
Dual (plus and minus) power supply only
Operating temperature range -40°C to +85°C -20°C to +70°C
Suitable Products