Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to design a system using CTR rank (K, L, or M) of PS2503-1?

Latest Updated:02/01/2008

Question:

Which CTR rank (K, L, or M) of PS2503-1 is produced in abundance?
(I would like to design a system using parts with stable supply.)

Answer:

It is difficult to say which CTR rank will be produced in abundance due to variation of the production volume of each rank in orders and variation that may occur during production.
If you can use products of any rank, we recommend purchasing products of all ranks, without specifying a single specific rank.

Suitable Products
Diodes for Constant Voltage
Photocouplers / Optocouplers