Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Does a thermal grease needs to be applied in 2SJ547 or the 2SK3212?

Latest Updated:09/02/2013

Question:

I'm considering using the 2SJ547 or the 2SK3212. Does thermal grease need to be applied? Also, is there any reference material?

Answer:

Grease needs to be applied in order to heighten the heat dissipation effect. For a general explanation, refer to 2.5 Mounting to the Heat Sink in the following document.

Suitable Products
Power MOSFETs for General Switching