Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What rating is the average on-state current?

Latest Updated:08/01/2007

Question:

What rating is the average on-state current?

Answer:

It is the average value of a current that is allowed to flow through a thyristor in the forward direction under specified temperature, current waveform and frequency conditions and is the average value in one cycle. Generally, it is the value when a single-phase half wave of 180° is allowed to flow at a commercial frequency of 50/60 Hz. Therefore, the triac does not have this rating.
Suitable Products
Diodes for Constant Voltage