Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What structures do arithmetic circuits that use amplifiers have?

Latest Updated:08/01/2009

Question:

What sorts of configurations do arithmetic circuits that use operational amplifiers have?

Answer:

The configuration of each type of arithmetic circuit is as follows:

(1) Adder circuit
This circuit outputs the sum of the input voltages. (The output voltage is within the rated range.)



(2) Subtractor circuit (differential amplifier circuit)
This circuit outputs the difference between the input voltages.



(3) Differential circuit
This circuit outputs the derivative of the input voltages.



Differential circuits are mainly used as active high pass filters, but the gain increases in proportion to the frequency, and the high frequency noise component is also amplified. Therefore, an incomplete differential circuit is often used to smooth out the rises of the output.



An incomplete differential circuit shows integration characteristics for the high frequency component.

(4) Integration circuit
This circuit outputs the integral of the input voltages.



Integration circuits are mainly used as active low pass filters.
Suitable Products
Operational Amplifiers
Industrial Network