Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What does this parameter prescribe of those operational amplifier?

Latest Updated:03/01/2007

Question:

The electrical specifications of a comparator are basically the same as those of an operational amplifier (Vio, Ib, etc.), except for the parameter "response time". What does this parameter prescribe?

Answer:

The response time prescribes the time between when a signal input to the comparator exceeds the reference voltage (Vref) and when the output amplitude reaches 50%.

Suitable Products
Comparators