Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

What is the method for accessing addresses of RAM pictograph display?

Latest Updated:08/01/2005


The pictograph display segments are driven by the uPD16432B, but what is the method for accessing addresses of the RAM for pictograph display?


Pictograph display refers to character display.
When reading 4.11 Commands in the uPD16432B Data Sheet, replace "character display RAM" with "pictograph display RAM".
In other words, in the mode setting, specify "001: Write to character display RAM," and set the addresses range to "00H to 07H."
Suitable Products
  • Este artigo foi útil?