Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

TPS-1 USB and PCI Support

Last Updated:06/01/2017

Question:

Does the TPS-1 support USB or PCI interfaces?

Answer:

The TPS-1 does not have a USB or PCI interface. However, if such interfaces are required, they can be implemented via a host CPU.
Suitable Products
TPS-1