Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

TPS-1 Software Support of SNMP Version 3

Last Updated:06/02/2017

Question:

Can the TPS-1 software support SNMP? Is it SNMP Version 1 or Version 3?

Answer:

The SNMP protocol has to be supported from Conformance Class B onwards and is implemented in the TPS-1 stack. The SNMP version information is described in the PROFINET V2.3 specification as “The SNMP services shall be derived from the IETF RFC 3418 (SNMP) standard." RFC 3418 means SNMP V3.
Suitable Products
TPS-1
  • Este artigo foi útil?