Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

TPS-1 Monitoring and Diagnostics for SFP Fiber via I2C

Last Updated:06/01/2017

Question:

Can the TPS-1 provide and monitor diagnostics for SFP fiber optic communication via I2C?

Answer:

Yes, this can easily be set in the TPS-1 configurator.
Suitable Products
TPS-1
  • Este artigo foi útil?