Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Function of TPS-1 TM0 and TM1 Pins

Last Updated:06/01/2017

Question:

What do the pins TM0 (Pin L4) & TM1 (Pin J10) do? Are these pins for manufacturer use only? Should I tie TM0 and TM1 to GND?

Answer:

The signals TM0 and TM1 are used for manufacturing and to select the TAPs for Boundary Scans. Pull-down with a 1K resistor during normal operation.
Suitable Products
TPS-1