Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Does the value to be set described on the User's Manual of UPD98410?

Latest Updated:08/01/2005

Question:

This question is about the minimum threshold value register for the total cell count for the UPD98410.
Does the value to be set have to be the value obtained with the equation described on the User's Manual?

Answer:

No, it does not have to be exactly the value obtained with the equation, but please set a value that is close to that value.
Suitable Products
BD/DVD Recorder
Digital Camcorder
Industrial Network