Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

sf_el_ux_comms Module Guide Resources

Last Updated:3/26/2018

Question:

Where can I find the references to module guide resources for the Express Logic USBX Communications Framework module on sf_el_ux_comms?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Communications Framework on USBX (TM) is a high-level API for Communications Framework applications that is implemented on the USBX Device Class CDC-ACM (Communications Device Class-Abstract Control Model). The Communications Framework uses the USB peripheral on the Synergy MCU device. This module is a replacement for the previous version, which was indicated as deprecated in SSP 1.2.0..

The Communications Framework on USBX has the following features:

  • High-level connectivity is supported on USB but is easily changed to UART or Ethernet connectivity without API modification
  • Supports channel locking for exclusive access
  • Supports USB high speed (HS) or full speed (FS) operation
  • Supports data transfer (DMA or DTC) peripheral operation
  • ThreadX®-aware implementation uses mutex and event flags internally

Module Guide

The Communications Framework on NX module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

Currently there is now module guide for the Communications Framework on NX module.

Module Guide Resources

  • Content provided as it becomes available.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products
SSP 1.2.0 and above
  • Este artigo foi útil?