Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

r_jpeg_decode Module Guide Resources

Last Updated:03/14/2018


Where can I find the module guide resources for the JPEG Decode HAL module on r_jpeg_decode?


The JPEG Decode HAL module doesn't have its own module guide. It is included in the sf_jpeg_decode module guide. The resources article for the sf_jpeg_decode module is available here.

The SSP User's Manual for SSP 1.4.0 (and beyond) has a detailed overview of the JPEG Decode HAL module in the Module Overviews section. This overview includes information on the API functions, configuration settings, an operational overview, use notes, limitations and a flow diagram of a typical application use. You can find the most recent version of the SSP User's Manual on the Renesas website here.

Suitable Products
  • Este artigo foi útil?