Pular para o conteúdo principal
Renesas Brasil - Knowledgebase

r_iwdt Module Guide Resources

Last Updated:02/27/2018


Where can I find the resources for the IWDT HAL module on r_iwdt?


Information on the module guide itself and the associated resources and known issues are available here.


The Independent Watchdog Timer (IWDT) HAL module is a high-level API for watchdog timer applications and is implemented on r_iwdt. The Watchdog Timer uses the IWDT peripheral on the Synergy MCU. A user can configure the timeout period, stop control on sleep and standby modes, window period and generation of event on WDT underflow or on refresh outside permitted window.

The IWDT HAL module supports the following features:

  • When the IWDT underflows or is refreshed outside of the permitted refresh window, one of the following events can occur:
    • Resetting of the device
    • Generation of an NMI
  • Supports the internal Watchdog timer peripheral (IWDT), which has its own clock source which improves safety.
    • Supports automatic hardware configuration after reset.

Module Guide

The IWDT HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the IWDT HAL module guide application note, application project and import guide are available here.

Module Guide Resources

The following application projects are available from the Renesas web site at the referenced url:

  • Thread Monitor Framework Module Guide - Application Project here.

The IWDT HAL module is used in the Monitoring Developer Examples available for the SK-S7G2. You can find a Knowledge Base article that describes the Developer Examples and how to use them here.

Known issues

  • Refer to the SSP release notes for known issues, available here.
Suitable Products
  • Este artigo foi útil?