Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

r_elc Module Guide Resources

Last Updated:06/19/2017

Question:

Where can I find the references to module guide resources for the ELC HAL module on r_elc?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Event Link Controller (ELC) HAL module is a high-level API for event linking applications and is implemented on r_elc. The ELC HAL module uses the ELC peripheral on the Synergy MCU. The ELC HAL module allows the developer to create events that link various peripherals within the Synergy MCU. The ELC HAL module APIs make it easy to create a link between two blocks (for example, from a timer to an ADC to control a periodic scan interval). By connecting various peripherals in this way, intelligent functions can be constructed that require little, if any, CPU intervention. 

The ELC HAL module supports the following features:

  • Create an event link between two blocks.
  • Break that event link between two blocks.
  • Generate one of two software events that interrupt the CPU.

Module Guide

The ELC HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the ELC HAL module guide application note, application project and import guide are available here.

Module Guide Resources

The following application projects are available from the Renesas web site at the referenced url.

  • HMI Brushless DC (BLDC) Motor Controller - Application Project here.
  • Renesas Bluetooth MCU (RL78/G1D) - Application Project here.
  • Bluetooth Low Energy on DK-S7G2 and DK-S3A7 - Application Project here.
  • Renesas Synergy™ Project DK-S3A7 Segment LCD Display Example here.
  • Renesas Synergy™ Project Checking Analog Inputs on the DK-S3A7 in Sleep Mode here.

Known issues

  • Refer to the SSP release notes for known issues, available here.

 

Suitable Products
SSP 1.2.0 and above
  • Este artigo foi útil?