Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

r_acmplp Module Guide Resources

Last Updated:02/27/2018

Question:

Where can I find the references to module guide resources for the Low Power Analog Comparator HAL module on r_acmplp?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The ACMPLP HAL module implements Analog Comparator APIs for signal processing applications on r_acmplp. It supports the ACMPLP peripheral available on the Synergy microcontroller hardware. A callback is available to signal the user application on transition events.

This module supports the following features:

  • Callback on rising edge, falling edge, or both
  • Configurable debounce filter
  • Option to include comparator output on VCOUT pin

 

Module Guide

The module guide is not yet available.

 

Module Guide Resources

There are currently no resources available for this module.

 

Known issues

  • Refer to the most current SSP release notes for any known issues.
Suitable Products
SSP
  • Este artigo foi útil?