Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Where can I find IBIS models for Synergy MCUs

Latest Updated:10/13/2016

Question:

Where can I get IBIS files for Synergy MCUs?

Answer:

IBIS models for Synergy S7G2 MCUs are available now for both 3.0 and 3.3V systems. You can find IBIS models in the Downloads Tab on the Synergy MCU web page. For example- this is the web page for the S7G2, just select Downloads and then select IBIS/BSDL and then click Search.

https://www.renesas.com/produc...7-series.html