Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the current SSP revision and when is the next release scheduled?

Latest Updated:5/14/2018

Question:

What is the current SSP revision and when is the next scheduled release?

Answer:

The current revision of SSP is 1.4.0 and the next release, 1.5.0, is currently scheduled for Sept 2018.
Suitable Products
SSP