Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What are the terms and conditions for the Renesas Rulz monthly Synergy application note idea kit give away?

Latest Updated:10/11/2016

Question:

What are the terms and conditions of the Renesas Rulz Monthly Synergy Application Note Idea Kit Give away?

Answer:

You can find the terms and conditions in the below attachment.

Offer is valid to residents of US, Canada and Mexico. Other restrictions may apply.

2016.03.04_Renesas_Synergy_SK-S7G2_Kit_Giveaway_T&Cs_(App._Note_Idea_Submission)_(U.S.,_Canada,_Mexico).pdf