Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What are some common Synergy Software Package compile errors and what can I do about them?

Latest Updated:10/04/2016

Question:

What are some common SSP compiler errors and what do I do about them?

Answer:

Here are some common compiler errors and the current work arounds for them.

1) If you get a compiler error related to JPEG, such as:

'g_jpeg_decode_cfg' undeclared here (not a function) (jpeg_decode_cfg_t const *) &g_jpeg_decode_cfg

It might be related to a know D/AVE2D issue. If you are using the D/AVE2D graphics driver make sure you place it in the HAL/Common layer and not in your thread. Putting it in your thread will generate an error.