Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

SSP Version 1.4.0 Usage Notes

Last Updated:03/30/2018

SSP Version 1.4.0 usage notes can be found in the attached PDF.

The usage notes include issues and workarounds for BSP, HAL, Framework, and Express Logic modules, as well as MCU implementation/SW architecture.

sspv140-v101_Additional-Usage-Notes.pdf

 

  • Este artigo foi útil?