Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

SK-S7G2 Weather Panel Design- any tricks I need to know about?

Latest Updated:10/04/2016

Question:

I'm using the SK-S7G2 Weather Panel Design Example- are there any tricks I need to know?

Answer:

Make sure when you are migrating the Weather Panel Design to SSP 1.1.0 that you check on the I2C configuration of the Touch Controller. It needs to be configured in Fast Mode not Standard Mode.