Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

NetX Duo FAQ

Latest Updated:10/04/2016

Question:

Is NetX Duo a 'real' dual stack implementation- are IPv4 and IPv6 supported simultaneously?

Answer:

Yes, NetX Duo (as the name implies) is a full dual stack implementation. At run time the mode is purely defined by the address space- if IPv4 addresses are used, the stack will us IPv4. If IPv6 addresses are used, the stack will use IPv6.

  • Este artigo foi útil?