Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is there an update to the BSP creator tool?

Latest Updated:10/04/2016

Question:

Is there an update to the BSP creator tool?

Answer:

The Rev 1.02 release of the BSP Creator is available from theSynergy Gallery under SSP Demos andApplications.

https://synergygallery.renesas.com/ssp/demo#read

Suitable Products
Synergy