Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

I get a compile error with the messaging framework when I have C++ code. What is going on?

Last Updated: 10/18/2017

Question:

I'm getting a compile error in the messaging framework with my C++ code. What is going on?

Answer:

There is a bug in the messaging framework code. This bug comes about because the name 'class' was used in the messaging framework as a variable name and it is a C++ reserved word. This bug has been identified and is fixed in SSP 1.3.0.