Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How so I enable static stack usage analysis and stack overflow checking for SSP?2

Latest Updated:09/15/2016

Question:

How do I enable Static Stack Usage Analysis or Stack Overflow Checking with a Synergy project?

Answer:

There are two GNU compile options that allow for these functions. You can find information on them here:

gcc.gnu.org/.../Static-Stack-Usage-Analysis.html

gcc.gnu.org/.../Stack-Overflow-Checking.html

They are added to you project here:

C/C++ Build -> Settings -> Miscellaneous -> Other compiler flags