Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I set-up USB drivers for Synergy CDC-ACM projects Windows 7 and Windows 8?

Last Updated:12/13/2017

Question:

How do I set-up USB drivers for Synergy CDC-ACM projects Windows 7 and Windows 8?

Answer:

The following USB driver installation process is used with Windows 7 and 8. For Windows 10, the driver is automatically found and installed. After starting the USB CDC-ACM project in debug mode the driver may show up as an Unknown Device in the Device Manager, under Other devices, as seen below.

USB Unknown.png

If this is the case, the driver will need to be installed. A signed driver that matches the USB device running in the application project is included in the downloaded project zip file. Save the .inf file, SynergyUSBCDC.inf, to a convenient location. Then follow these simple steps:

1. Right click on the Unknown device in Device manager and select Update Driver Software...

2. Select Browse my computer for driver software

3. Select Let me pick from a list of device drivers on my computer

4. Scroll down and select Ports (COM & LPT) and click Next

USB COM.png

5. Click on Have Disk...

6. When the Install From Disk dialog box comes up, Browse to the folder that holds the .inf file (SynergyUSBCDC.inf), select the file and click Open, then OK.

7. The signed driver should show up in the Model list as Synergy USB CDC/ACM. Click Next.

8. Ignore any Warnings and continue to install the driver.

9. The driver should now be installed and will show up in the Ports (COM & LPT) list as seen below.

USB CDC-ACM.png

SSP