Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I select the correct IAR compiler for my Synergy project if I have multiple IAR installations?

Latest Updated:10/04/2016

Question:

How do I select the correct iAR compiler in the Synergy Platform if I have multiple IAR installations?

Answer:

Here is how you make the required change, within e2 studio, to reset the IAR selection: 

Window->Preferences

Preferences->IAR Embedded Workbench

Browse to the correct path to IAR Embedded Workbench by pressing "Browse" and navigating to the correct directory.

Once done, the proper version is in boldface in the plugin manager.