Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I install e2 studio and SSP on a computer without an Internet connection using the offline installer?

Latest Updated:10/04/2016

Question:

How do I install e2 studio and SSP on a computer without an internet connection?

Answer:

You can use the e2 studio offline installer to install without an internet connection. The SSP installer can be transferred to a computer and installed offline as well. The compilers need to be downloaded separately and transferred also. You can find the GCC compiler here:

You can find a Synergy-compatible version of the GCC toolchain here:

https://launchpad.net/gcc-arm-embedded/+milestone/4.9-2015-q3-update 

Double check, via the installation guide and release notes that this version of GCC is the correct one for your version of e2 studio and SSP since GCC is periodically updated.