Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I get a license for the IAR Embedded Workbench for Renesas Synergy?

Last Updated:03/14/2018

Question:

How do I get a license for the IAR Embedded Workbench for Renesas Synergy (IAR EW for RS)?

Answer:

The process for obtaining and installing the license is described below:

1) If you download and install Embedded Workbench, the first time you start the program you see the following Welcome Screen:

IAR_Welcome.jpg

2) Click on Next to get an evaluation license. You will see the following Registration Screen:

IAR_Register.jpg

3) Go to the following URL to get a license.

https://register.iar.com/specialedition/RenesasSynergy

That url brings up the following dialog and you can enter your email address to get an Evaluation license sent to you.

IAR_Email.jpg

4) Enter the License number into the Registration window shown previously and click Next. Your license will be installed and the software will be ready to use.

5) To create a Permanent License follow these easy steps:

  • In IAR EW for Synergy, select Help > License Manager.
  • In the IAR License Manager, select License > Check for License Renewal.
  • Select your license number and click the Check selected licenses button.
  • The IAR License searches for license renewals for your license.
  • After the IAR License Manager has retrieved the updated license keys, click the Renew selected button.
  • The IAR license Manager presents you with the renewal results.
Suitable Products
SSP