Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I correct the failure of sf_el_nx_comms to respond when using multiple instances?

Last Updated:04/16/2018

Question:

How do I correct the failure of sf_el_nx_comms to respond when using multiple instances in an application?

Answer:

Applications should not use multiple instances of sf_el_nx_comms in an application. In fact, sf_el_nx_comms is not recommended for new designs since it has been replaced with sf_comms_telnet. Use sf_comms_telnet instead since it doesn't exhibit this issue. However, it is not a recommended design practiced to use multiple IP Instances since there are global variables involved which will result in undefined behavior.
Suitable Products
SSP