Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I implement picture blending without using multiple canvases in GUIX and SSP?

Latest Updated:10/02/2016

Question:

Is there an easy way to implement picture blending without using multiple canvases in SSP with GUIX?

Answer:

You can implement picture blending with a single canvas by using an array of pixel maps and a changing alpha blend setting. The attached example design illustrates this approach for the SK-S7G2. Comments in the code (src/guix_gen/gx_studio_events.c) describe the approach.

/@api/deki/files/1830/s7_sk_gx_blend_demo_1_0_0g_small.zip?origin=mt-web