Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How do I Create a Synergy Custom Board Support Package?

Last Updated: 11/20/2015

Question:

How do I create a custom Board Support Package (BSP) for a Synergy project?

Answer:

You can easily create a custom BSP by following the guidelines shown in this application note.