Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Where can I find the SSP Thread-X and related user manuals?

Last Updated: 04/21/2016

Question:

Where can I find the ThreadX and other related Users Manual for the Synergy SSP?

Answer:

The ThreadX Users Manual is found on the Synergy Gallery on the SSP top level tab. Use the Documentation low level tab and the zip file of all the SSP ThreadX related User Manual- ThreadX, USBX, FileX, NetX, etc are collected in the zip file on the right side tool bar.

You can also find all of the ThreadX related Users Manuals for NetX AutoIP, NetX DNS, NetX HTTP, etc here: https://synergygallery.renesas.com/ssp/support#read on the right hand side bar as a zip file.

 

 

 

  • Este artigo foi útil?