Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

FAQ for S3A1 and SSP 1.4.0 Launch

Last Updated:04/12/2018

Question:

What release information is available for SSP 1.4.0?

Answer:

Section 1: S3A1 MCU Group

1:    Where can I learn about the features of the S3A1 MCU group?

  • Please visit renesassynergy.com/s3a1 to view the block diagram of the S3A1 MCU group.
  • Please visit renesassynergy.com/mcuglossary to learn about the peripherals available in the S3A1 MCU group.

2:    Where is documentation (user manual, datasheet, design data, etc.) of S3A1 MCU group located?

  • Please visit renesassynergy.com/s3a1. Scroll down to the Products section, find the part of interest and locate the pointer to it’s documentation below the part number.

3:    What hardware kits are available to evaluate S3A1 MCU group?

  • Target Board Kit TB-S3A1 provides access to all pins, standardized expansion ports, and preinstalled demo software for S3A1 MCU group. Please visit renesassynergy.com/tb-s3a1 to learn more about the kit.

4:    Where is documentation (user manual, datasheet, design data, etc.) of TB-S3A1 Target Board Kit located?

  • Please visit renesassynergy.com/tb-s3a1 to learn more about the kit and scroll down to Documentation & Support section to find the quick start guide, user manual and design data.

5:    From where can the TB-S3A1 Target Board Kit be obtained?

  • Please visit renesassynergy.com/tb-s3a1 to learn more about the kit and scroll down to Documentation & Support section below which you can find the pointers to the distributors who are selling TB-S3A1.

6:    From where can I get technical support for S3A1 MCU group?

  • Please visit renesassynergy.com/support and select from various options to get self-help and personalized technical support.

 

Section 2: SSP 1.4.0

1:    What are the key features and improvements in SSP 4.0 over 1.3.x?

  • For list of all the features, please refer to the SSP 1.4.0 release notes. They can be obtained from the Documentation & Support section of the renesassynergy.com/ssp

2:    Where can SSP 1.4.0 be downloaded from?

  • SSP 1.4.0 can be download standalone or as a part of Platform Installer (included SSP, e2studio or IAR Embedded Workbench for Synergy). Both can be downloaded from the Download section of the renesassynergy.com/ssp

3:    What development tools/environments can be used to develop with SSP 1.4.0?

  • You can select from two development tools/environment. e2 studio ISDE or IAR Embedded Workbench for Synergy.

4:    From where can the development environment can be obtained?

  • The development environment can be downloaded and installed separately from SSP or they can be installed along with SSP by using the platform installer.
  • The Platform Installed can be downloaded from the Download section of the renesassynergy.com/ssp
  • The e2 studio ISDE can be downloaded from the Download section of the renesassynergy.com/e2studio
  • The  IAR Embedded Workbench for Synergy can be downloaded from the Download section of the renesassynergy.com/ewsynergy

5:    Where is the documentation of SSP 1.4.0 located?

  • Documentation including user manual, datasheet, release notes, module guides, etc. can be obtained from the Documentation & Support section of the renesassynergy.com/ssp

6:    From where can I get technical support for SSP 1.4.0?

  • Please visit renesassynergy.com/support and select from various options to get self-help and personalized technical support.

 

Suitable Products
SSP
  • Este artigo foi útil?